AnsweredAssumed Answered

configuring cubemx with F429ZI and ethernet

Question asked by Andrew Chin on Nov 21, 2017
Latest reply on Nov 21, 2017 by Andrew Chin

I am trying out ethernet with UDP. However, when I generate the files through cube mx, I am unable to get it working like they do in UM1713. 

 

I tried to compile a project, but it does not like "ethernetif_input(&gnetif)". It seems that gnetif is not used anywhere. 

 

Also, there is no Netif_Config called, so I tried calling it as it is in the manual, but it did not like that either. 

 

So, I looked for a demo, and I found one with the STM324XG_EVAL. The first thing I noticed was that it did not even include these files in the code generation:

 

#include "lwip/opt.h"
#include "lwip/init.h"
#include "lwip/netif.h"
#include "lwip/timeouts.h"
#include "netif/etharp.h"
#include "ethernetif.h"
#include "app_ethernet.h"
#include "udp_echoserver.h"

 

Is there something I was supposed to do in CubeMX to include all the needed files?

Outcomes