AnsweredAssumed Answered

help httpserver on nucleo board: I pay for it

Question asked by dieter 123 on Nov 22, 2017
Latest reply on Nov 22, 2017 by AvaTar

Hi

I am late in y project and need some help with a HTTP server.

This is what I need:

a webserver for FW download which also gives me the opportunity to change IP Address and Netmask, ideal on a nucleo stmf429zi board, but any other would do as well.

 

One of the ST example projects should be taken as starting point, like this one:

STM32Cube_FW_F4_V1.16.0\Projects\STM324xG_EVAL\Applications\LwIP\LwIP_IAP

A teamviewer session should be

 

Deliverables: 

- firmware project : WEbserver IAP to upload FW , set netmask, IP address , IPV4

- Git repository with 2 commits: example code of ST + all changes

- an application FW which just blinks some leds

- 1 hour team viewer session demo about what needed to be changed and why.

Any one interested? send me a PM

Thx

Outcomes