AnsweredAssumed Answered

UART DMA read firing required only once or every time?

Question asked by Abhishek Kumar on Nov 20, 2017

MCU: STM32F777II

I have configured DMA for RX on the UART as:

 

/* UART7 DMA Init */
/* UART7_RX Init */
hdma_uart7_rx.Instance = DMA1_Stream3;
hdma_uart7_rx.Init.Channel = DMA_CHANNEL_5;
hdma_uart7_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_uart7_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_uart7_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_uart7_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_uart7_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_uart7_rx.Init.Mode = DMA_CIRCULAR;
hdma_uart7_rx.Init.Priority = DMA_PRIORITY_MEDIUM;
hdma_uart7_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;

 

Just wanted to when I fire off a DMA read using the HAP api:

HAL_UART_Receive_DMA(&UART_DOWN_USB_TO_SERIAL, (uint8_t*)&holder, 1);

 

Do I need to call  HAL_UART_Receive_DMA() again in the HAL_UART_RxCpltCallback callback function, or it was required only once provided I need to continue reading it infinitely?

Outcomes