AnsweredAssumed Answered

External SRAM with STM32L496

Question asked by chris puglia on Nov 17, 2017
Latest reply on Nov 24, 2017 by Madhan Mohan Gundluru

Hello,

 

I am trying to find examples of code where the external SRAM is mapped using the linker file. I saw an example of it being done here (Declaring variables in External SRAM ). However, all the uses of the SRAM eg.[the  HAL_SRAM_Write_32b() function] in the example code make use of locking. If anyone has examples of using external RAM as general purpose RAM it would be greatly appreciated. 

 

FYI this is being done on the STM32L496G-DISCO board

Outcomes