AnsweredAssumed Answered

Is there anyone who worked with USB HID Cubemx

Question asked by -----????_---- ---??as on Nov 17, 2017

I just want to know what is the max speed he could get from USB HID Class.For example Can he send 128 Bytes in 2 ms(64 Bayt x 2 Message).I can not send the second message without waiting for  ~750 ms after sending the first.I am using cubemx and his USB HID class.Is it normal?

 

 

USBD_CONF_Exported_Defines :

/*---------- -----------*/
#define USBD_MAX_NUM_INTERFACES 1
/*---------- -----------*/
#define USBD_MAX_NUM_CONFIGURATION 1
/*---------- -----------*/
#define USBD_MAX_STR_DESC_SIZ 512
/*---------- -----------*/
#define USBD_SUPPORT_USER_STRING 1
/*---------- -----------*/
#define USBD_DEBUG_LEVEL 0
/*---------- -----------*/
#define USBD_SELF_POWERED 1
/*---------- -----------*/
#define USBD_CUSTOMHID_OUTREPORT_BUF_SIZE 64
/*---------- -----------*/
#define USBD_CUSTOM_HID_REPORT_DESC_SIZE 189
/****************************************/
/* #define for FS and HS identification */
#define DEVICE_FS 0

Outcomes