AnsweredAssumed Answered

Quick start  STM32F7

Question asked by Andrij Markovsky on Nov 14, 2017
Latest reply on Nov 14, 2017 by Clive One

1. I have necessity force to start STM32F7 after reset as fast as possible.
How to do it correctly using HAL or Low-layer drivers?

 

In "Description of STM32F7 HAL and Low-layer drivers" I find in chapter "FAQs"

Follow the sequence below to use the APIs provided in the HAL drivers:
1. Call HAL_Init() function to initialize the system (data cache, NVIC priority,…).
2. Initialize the system clock by calling HAL_RCC_OscConfig() followed by
HAL_RCC_ClockConfig().
3. Add HAL_IncTick() function under SysTick_Handler() ISR function to enable polling
process when using HAL_Delay() function
4. Start initializing your peripheral by calling HAL_PPP_Init().
5. Implement the hardware low level initialization (Peripheral clock, GPIO, DMA,..) by
calling HAL_PPP_MspInit() inxx_hal_msp.c
6. Start your process operation by calling IO operation functions.

As i understood after the resett, the STM32F7 series is running on HSI clock(It means 16MHz).
And runtime envioroument called on HSI frequncy.
==========
Issues.
==========
1. I have necessity force to start STM32F7 after reset as fast as possible.
How to do it correctly using HAL or Low-layer drivers?

2.I have necessity to check and initialize External SRAM and SDRAM,
before running "C-runtime envioroument".
Is it possible using HAL or Low-layer drivers?

For experiments I used Evaluation board with STM32F746G-EVAL2,
Firmware: J-Link ARM / Flasher ARM V4.

 

My best regards,
Andrij Markovsky

Outcomes