AnsweredAssumed Answered

[bug] STM32CubeMX generate lot of .tmp files in source directory

Question asked by Jan Breuer on Nov 14, 2017
Latest reply on May 3, 2018 by houda ghabri

After creating the project, there are lot of .tmp files in the source directory. They are always regenerated. I have selected to generate all code in main.c instead of separate file for each peripheral.

 

e.g. gpio.tmp

#n/** Configure pins as #n #t#t #t* Analog #n #t#t #t* Input #n #t#t #t* Output#n #t#t #t* EVENT_OUT#n #t#t #t* EXTI
*/

static void MX_GPIO_Init(void)
{
#n
#n#t/* GPIO Ports Clock Enable */
#tLL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOA);
#tLL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOB);
#n
}
#n

 

MCU: STM32F030F4Px

PC OS: Linux

CubeMX version: 4.23.0

Firmware package: STM32Cube FW_F0 V1.9.0

Outcomes