AnsweredAssumed Answered

[bug] STM32CubeMX 4.23.0 does not copy startup.s

Question asked by Jan Breuer on Nov 14, 2017
Latest reply on Nov 15, 2017 by Imen D

I have selected option for "STM32 Firmware Library package" -> "copy only the necessery library files".

I'm using just LL libraries and GPDSC project.

All files ware generated without error but no startup file was present in the project, only blank directories "arm", "gcc" and "iar" ware created in directory "Drivers/CMSIS/Device/ST/STM32F0xx/Source/Templates/"

 

On the other hand, it copies "system_stm32f0xx.c" in "Templates" directory, which is not needed, because similar file is generated with the same name and functionality to the "Src" directory. 

 

 

MCU: STM32F030F4Px

PC OS: Linux

CubeMX version: 4.23.0

Firmware package: STM32Cube FW_F0 V1.9.0

Outcomes