AnsweredAssumed Answered

STM32F7 USB / HAL / DMA

Question asked by Eugene Solo on Nov 11, 2017
Latest reply on Dec 7, 2017 by Eugene Solo

I'm doing research on USB lib v2.4.2 and HAL (checked 1.6.0 and 1.8.0), trying to understand how it's internals are working. Target chip is STM32F746, target mode is FS (because of internal PHY).

 

I'm stuck at this function from stm32f7xx_ll_usb.c:

HAL_StatusTypeDef USB_WritePacket(USB_OTG_GlobalTypeDef *USBx, uint8_t *src, uint8_t ch_ep_num, uint16_t len, uint8_t dma)
{
  uint32_t count32b= 0 , i= 0;
 
  if (dma == 0)
  {
    count32b =  (len + 3) / 4;
    for (i = 0; i < count32b; i++, src += 4)
    {
      USBx_DFIFO(ch_ep_num) = *((__packed uint32_t *)src);
    }
  }
  return HAL_OK;
}

what this function will do if parameter 'dma' is not equals to 0? I mean, if DMA is meant to be used, how and when data will be written to FIFO? How data is extracted from FIFO if reading function using same approach (Note: commented documentation says about parameter 'dma' but obviously its not even mentioned in function proto; same with ch_ep_num - this function reas from DFIFO0 only!):

/**
  * @brief  USB_ReadPacket : read a packet from the Tx FIFO associated
  *         with the EP/channel
  * @param  USBx : Selected device  
  * @param  src : source pointer
  * @param  ch_ep_num : endpoint or host channel number
  * @param  len : Number of bytes to read
  * @param  dma: USB dma enabled or disabled
  *          This parameter can be one of these values:
  *           0 : DMA feature not used
  *           1 : DMA feature used  
  * @retval pointer to destination buffer
  */
void *USB_ReadPacket(USB_OTG_GlobalTypeDef *USBx, uint8_t *dest, uint16_t len)
{
  uint32_t i=0;
  uint32_t count32b = (len + 3) / 4;
 
  for ( i = 0; i < count32b; i++, dest += 4 )
  {
    *(__packed uint32_t *)dest = USBx_DFIFO(0);
    
  }
  return ((void *)dest);
}

 

Could someone clarify exactly how DMA USB is working? Does it work at all? RM says that registers DIEPDMAx and DOEPDMAx are "only to USB OTG HS". Can FS work with DMA or only by crude copiing, or what?


My wild guess is: to transfer data between DFIFO and application I should use DMA mem-to-mem function, am I right?

Outcomes