AnsweredAssumed Answered

cubemx

Question asked by Robert Gosztyła on Nov 9, 2017

Hi

 

I'm using newest possible CubeMX version. Trying to generate project for some environment, in this case SW4STM32 (however tool does not matter) and got this window. Code is generated, only project cannot be done. Java installed is 9.0.1.

 

 

Checking Java output got something like this:

 

2017-11-09 19:40:01,978 [INFO] ProjectBuilder:1369 - Project Generator version: 2.26.0
2017-11-09 19:40:01,988 [INFO] ConfigFileManager:343 - The Die is : DIE410
2017-11-09 19:40:02,013 [INFO] ToolchainGenerator:103 - [Project Generator] Problem in the project generation
java.lang.ClassCastException: parsers.SysWbParser cannot be cast to parsers.FromScratchParser
        at convertor.Convertor.convert(Convertor.java:546)
        at convertor.Convertor.generate(Convertor.java:349)
        at com.st.microxplorer.plugins.projectmanager.model.ToolchainGenerator.generate(ToolchainGenerator.java:99)
        at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createToolChainFolders(ProjectBuilder.java:1408)
        at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:508)
        at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:41)
2017-11-09 19:40:02,021 [INFO] ProjectBuilder:1424 - Time for Generating toolchain IDE Files: 44mS.
2017-11-09 19:40:02,022 [ERROR] ProjectBuilder:1430 - Error in Project Generation
2017-11-09 19:40:02,022 [ERROR] ProjectBuilder:524 - Error in Project Generation

 

Any help is welcome.

BR, Robert

Outcomes