AnsweredAssumed Answered

STM32F030X8 alternate function unclear

Question asked by Valeriy Horash on Nov 8, 2017
Latest reply on Nov 9, 2017 by Uwe Bonnes

In the STM32F030X8 datasheet the PortB pin 15 alternate function AF0 is both SPI1_MOSI and SPI2_MOSI

(see table 13 on page 35 of en.DM00088500.pdf). The pin 15 is just an example - there are more of such.

How can this be resolved? Is there some other register that specifies the SPI module to connect to the pin?

Outcomes