AnsweredAssumed Answered

32F769IDISCOVERY UART7 usage

Question asked by Joerg Wagner on Nov 8, 2017
Latest reply on Nov 8, 2017 by Joerg Wagner

I selected the 32F769IDISCOVERY board in CubeMX.

Why is UART7 in CubeMX disabled?

The pins in the conflicts list are not mapped or active.

For my app I need the Arduino Pin D3 which is UART7_RX.

I studied the schematics and do not find any conflict with other devices.

When I force to use PF6 for RX7 and PF7 for TX7 the UART7

can be activated in CubeMX.

But my app does not receive a character in the callback function (IT is used).

Thank you.

Outcomes