AnsweredAssumed Answered

Use of WHITE_LIST

Question asked by jamp on Nov 1, 2017
Latest reply on Nov 7, 2017 by jamp

Hello,

 

I am using two bluenrg-1 devices, one of them working as a slave and other working as a master. I would like to know if there is any example I can use where the white_list is used or if anyone can give me some ideas.

What I am doing now is on the central side, when the slave is advertising (ADV_IND) and the master received the hci_le_advertising_report_event() I will get the Address and type address and add the information of that device using the function aci_gap_add_devices_to_resolving_list().

Once I have added the device I will start creating the connection using the function aci_gap_start_general_connection_establish_proc().

Is that procedure correct or should I do it in a different way?

 

Thank you

Outcomes