AnsweredAssumed Answered

I-CUBE-LRWAN v1.1.2 - Set Tx Power?

Question asked by Andrew Neil on Oct 30, 2017
Latest reply on Dec 8, 2017 by Andrew Neil

Is it possible to "manually" configure the Tx Power level using the I-CUBE-LRWAN v1.1.2 software?

 

I can see that the End_Node demo enables Adaptive Data Rate:

/* !
*Initialises the Lora Parameters
*/

static  LoRaParam_t LoRaParamInit= {TX_ON_TIMER,
                                    APP_TX_DUTYCYCLE,
                                    CLASS_A,
                                    LORAWAN_ADR_ON,
                                    DR_0,
                                    LORAWAN_PUBLIC_NETWORK,
                                    JOINREQ_NBTRIALS};

 

But, if I disable it, I don't see how/where I'd set the Tx power level.

 

Related: With ADR enabled, is there a way for the node to limit the maximum Tx power level?

Outcomes