AnsweredAssumed Answered

LIS2DW12, how are the interrupt pins internally connected?

Question asked by blabla.blabla on Oct 30, 2017
Latest reply on Oct 30, 2017 by blabla.blabla

LIS2DW12, if interrupt pins (INT1 & INT2) are configured to open-drain mode, will they still work if the VDDIO supply is cutoff? (and the interrupt pins are pulled up to another supply voltage) and the VDD is still connected to 1,8V ? Will the VDD voltage still control the open-drain pins or is it completely fed by the VDDIO voltage?

Outcomes