AnsweredAssumed Answered

PWM output initialization problem

Question asked by Greg73 on Mar 8, 2012
Hi!

I am outputting a PWM signal from TIM3/ch1 (pin PA6). The signal would be a clock signal for external chip btw and I need it to be switchable. All is working nicely. However, after the initialization code (see below), the initial state of the PWM pin is going high but I need it to stay low.
How can I change that? I stepped through the TIM_OC1Init function in the standard library and found that the output goes high when I enable the output in TIM3->CCER (CC1E).

Thank you in advance!

void Init_PWM(void){
   
  /* Compute the prescaler value */
  PrescalerValue = (uint16_t) (SystemCoreClock / 24000000) - 1;
  /* Time base configuration */
  TIM_TimeBaseStructure.TIM_Period = 960;
  TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue;
  TIM_TimeBaseStructure.TIM_ClockDivision = 0;
  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
 
  TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
   
   
  /* PWM1 Mode configuration: Channel1 */
  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
  TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
  TIM_OCInitStructure.TIM_Pulse = CCR1_Val;
  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
 
  TIM_OC1Init(TIM3, &TIM_OCInitStructure);
 
  TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Enable);
 
   
 
  TIM_ARRPreloadConfig(TIM3, ENABLE);
 
  /* TIM3 enable counter */
  //TIM_Cmd(TIM3, ENABLE);
   
 
   
}//Init_PWM

Outcomes