AnsweredAssumed Answered

Adding UART, SPI port to EEPROM Emulation example

Question asked by Luis Ornelas on Oct 27, 2017
Latest reply on Feb 23, 2018 by Clive One

Hi, I have two projects. One with all the features I want to have: UART, SPI and other protocols to initialize the LCD; it was built with STM32 CUBE MX. The other project is the EEPROM Emulation modified to read some values after power on. Both are working, I want to join both to build just one project. The problem Im facing is, I tried to configure all the peripherals, the code compiles but the board doesn't do anything else but only the eeprom emulation feature. Do you know what I can be missing? 

Outcomes