AnsweredAssumed Answered

Eclipse - IAR EWARM - Eclipse import project - java.lang.NullPointerException error

Question asked by kaminski.gregorio on Oct 7, 2014
Latest reply on Oct 16, 2014 by nouha

I´m trying to import a STM32F401-Discovery Demo Project into the Eclipse IDE with errors.

stsw-stm32136 STM32F401-Discovery_FW_V1.0.0

I attached some pictures  for reference only.

Some steps that I was following:

1.) I have instaled plug-ins into Eclipse Kepler  from http://eclipse-update.iar.com/
The plugin supports IAR Embedded Workbench for ARM (EWARM) 6.50.x/6.60.x/6.70.x/7.10.x.

2.) After install and the reset I run again the Eclipse with and a plugin error.
"An error occurred while initializing the SDK IAR Toolchain for ARM - 6.x"

3.) When I´m trying an import following: Import->IAR Embedded Workbench->Import IAR Embeded Workbench project
(see the attached pictures for ref.), another error happens:

Failed to import project - An error occured during import:
java.lang.NullPointerException
Refer to the error log for more details.

  
I don´t know if evetually it is a problem from java due it was updated to Java Version 7 Update 67 or from IAR plugins or there are a problem on the project example: STM32F401-Discovery_FW_V1.0.0
I would like to say that I had already managed to import ok into another environment few months ago.

Have you the same problem? What is the miss on this procedure?
I´m sharing some information about this issue but Any help are welcome, please.

Thanks in advance,

Greg/Brazil
=====================================================
STM32F401C-DISCO - IAR Embedded Workbench 7.10.1.6735 - Eclipse Kepler 4.3.2 
- Java 7 - 67 - Portugues/Brazilian language, Windows XP 32 bits - environment

 

Outcomes