AnsweredAssumed Answered

CubeMX 4.23.0 bugs NUCLEO-H743ZI

Question asked by Joerg Wagner on Oct 25, 2017
Latest reply on Feb 16, 2018 by Joerg Wagner

Hi guys.

1.)

I already mentioned a bug in the previous CubeMX release.

Enabling Ethernet CubeMX reserves

PB12 for ETH_TXD0

and

PB11 for ETH_TX_EN

and writes the wrong settings in ethernetif.c

 

But it must be:

PG13 for ETH_TXD0

and

PG11 for ETH_TX_EN

 

2.)

The speed setting should be at least HIGH or VERY_HIGH but it is set to:

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW

 

3.)

A new project with the button checked "Initialize all peripherals with their default Mode"

will not find a solution if setting the clock to 400 MHz. Setting the dividers by hand works.

Solution: Uncheck USB_OTG_FS, because the clock solution process does not find a goal for 48 MHz.

 

4.)

Sometimes I had the situation: I disabled "USB_OTG_FS" but it was still green and listed under Configuration.

 

 

- Joerg -

Outcomes