AnsweredAssumed Answered

CubeMX on Linux fails to generate FSMC MSP code

Question asked by frackers on Oct 24, 2017
Latest reply on May 14, 2018 by Mohamed Mansouri

Running latest 4.22.1 STM32CubeMx on both *buntu and Windows 7 and the generated stm32f4xx_hal_msp.c is totally different. The HAL libraries in both cases are STM32Cube_FW_F4_V1.16.0. 

With the Linux version, the following functions are missing:

  • HAL_FSMC_MspInit
  • HAL_SRAM_MspInit
  • HAL_FSMC_MspDeInit
  • HAL_SRAM_MspDeInit

which results (not surprisingly) a totally useless build.

This needs to be fixed urgently as I only have part-time access to a single windows machine to create the code if I change any pinouts etc.

Outcomes