AnsweredAssumed Answered

Write into flash while USART interrupt executed

Question asked by Clemens Ehm on Oct 23, 2017
Latest reply on Oct 26, 2017 by Clive One

Hello,

 

I have some trouble to write into the flash of my stm32f091. I can send via usart a lot of commands to the µC, interprete and execute them finally. One command is to write some data into the flash but if I write and the usart is still receiving data, the communication is totally dead - only mcu reset helps.

The only "solution" which doesn't crash the communication is to deactivate the usart with USART1->CR1 &= ~USART_CR1_UE; before I write into flash and re-enable it after the flash operation - but that's not a real solution cause I will lose data/commands.

 

What I tried:

- Moving the vector table into SRAM

- Disable the usart interrupt (NVIC_DisableIRQ(USART1_IRQn);)

- __disable_irq(); before the flash operation

 

Without any effect. The linker script has the following settings:

MEMORY
{
FLASH (rx)      : ORIGIN = 0x8000000, LENGTH = 128K
UNUSED (rx)      : ORIGIN = 0x8020000, LENGTH = 128K
RAM (xrw)      : ORIGIN = 0x200000C0, LENGTH = 32K - 0xC0
}

 

I always write into the UNUSED section, not the FLASH where the running firmware is stored.

The best solution would be to disable the interrupt for the flash-write-time, the mcu buffering all incoming packages for the moment and after re-enabling the interrupt I receive the buffered data. Is that somehow possible or you have any other useful hints for me?

 

Thanks

Outcomes