AnsweredAssumed Answered

BlueNRG-1 PWM and resources usage

Question asked by Micha Valach on Oct 24, 2017

Hello,

 

I’d like to generate automatic code for PWM on the BlueNRG-1 chip.

 

While using the latest Cube-MX, I couldn’t find neither the evaluation board STEVAL-IDB007V1 nor BlueNRG-1 chip, ioc files.

1. Is it possible to get the ioc file of the BlueNRG-1 running on the STEVAL-IDB007V1 ?

I already selected another Cortex-M0 µ-Processor 32 pin, however the code generated seems a bit different, from the specific BlueNRG-1 examples code!!

2. How can I verify what are the resources using by the bluenrg_stack_lib.a file, for example: Is timer-0 or 1 available? Which timer should I use for PWM so that the ch1 output will be on IO3?

3. Can I modify the values of Tim1 or Tim0?

 

Please advise,

 

Thanks In Advance,

 

Best regards,

 

Micha Valach

Outcomes