AnsweredAssumed Answered

STM32F407 USB MSC example code

Question asked by Simon Rees on Oct 23, 2017
Latest reply on Oct 23, 2017 by Simon Rees

I am looking at running USB Host software on the STM32F407VG device, probably using the STM32F407G-DISC1 eval board but haven't ordered it yet.

I downloaded the STM32_USB-Host-Device_Lib_V2.2.0 example code from the link on the device web page.

I built the HOST MSC example, for IAR EWARM,  and it built with no issues. However I noticed that it was configured for the the F107 and not the F407 that I want.

This is as far as I have got so before I go any further can I check that this will build for the F407.

Do I just change the CPU target in the project options or do I need to change anything else?

Outcomes