AnsweredAssumed Answered

UTF-8 source code merge bug at CubeMX Genarate Code

Question asked by Yasuhiro Hirano on Oct 23, 2017
Latest reply on Feb 8, 2018 by Jeanne Joly

Hello.

I am troubled with garbled characters of CubeMX's code generation function.

 

The version of CubeMX is 4.22.1.

The development environment is SW4STM32.

The reproduction method is explained below.

 

1. Generate the code with CubeMX.

2. Open the project with SW4STM32 and change the character code of the project to UTF-8.

3. Open main.c and add Japanese characters to the USER CODE area.

Before garbling

4. Quit SW4STM32.

5. Start CubeMX and generate the code again without changing anything.

6. When SW4STM32 is started and main.c is opened, it can be confirmed that garbled characters are occurring. You can also check garbled characters in the text editor.

After garbling

 

From this, I think that CubeMX has the cause of garbled characters.

Is there any workaround?

 

Best Regards

Yas

Outcomes