AnsweredAssumed Answered

stm32CubeMX cant install on Linux 64bit

Question asked by Martin Bachtold on Oct 19, 2017
Latest reply on Dec 3, 2017 by Nikolay Mernik

Hi all

 

I'm new to stm32 and have troubles to install the CubeMX Standalone and Eclipse Plugin.

 

I've downloaded the archive fro st.com, unarchive made the installer executable but the installer dosn't start.

When i tried to start from command line 

 

[tino@archlinux en.stm32cubemx]$ ./SetupSTM32CubeMX-4.22.1.linux  
bash: ./SetupSTM32CubeMX-4.22.1.linux: No such file or directory

I've triy also as Eclipse plugin, Its running but after some time the eclipse window starts flicker.

 

java version "1.8.0_152"
Java(TM) SE Runtime Environment (build 1.8.0_152-b16)
Java HotSpot(TM) 64-Bit Server VM (build 25.152-b16, mixed mode)

Outcomes