AnsweredAssumed Answered

No build config for F303RE in IAR

Question asked by Fredrik Pande on Oct 17, 2017
Latest reply on Jan 17, 2018 by Fredrik Pande

I am experiencing some issues running the FOC SDK v4.3.

 

My HW-setup:

Control board: NUCLEO - STM303 (ST part number)

Power board: X-NUCLEO-IHM08M1 (ST part number)

PMSM motor

 

IDE: IAR

 

Currently I am able to compile and download code to the F303RE, however the motor only spins a short period of time, and then stops, requiring a reset with the black reset button in order to make it start running again using the user button (blue) on the F303RE. I am not sure what the problem is, but I notice that there is no build configuration for the F303RE.

 

Currently I open STM32 PMSM FOC LIB\Web\Project\EWARM\STM32F30x_Workspace.eww and build using STM32303C-EVAL_SINGLEDRIVE as option in the drop-down menu, please see attached pic.

 

Why is there no build config for F303RE in IAR drop-down menu?

 

Should I even be able to compile and download to target when the build config is wrong?

 

My problems could have all types of sources obviously, but I would like to ensure that I am using the correct build config at least.

Attachments

Outcomes