AnsweredAssumed Answered

I-Cube LoRaWan V1.1.2 with STM32L151CC

Question asked by Jérémy Da Silva on Oct 12, 2017
Latest reply on Oct 12, 2017 by Clive Two.Zero

Hi everybody,

 

I made my PCBA with a STM32l151CC and a SX1272 from Semtech in order to make a LoRa Accessory.

 

I use Cube MX software to configure all the peripheral of my accessory (SPI, ADC, RTC, etc.) and I add all the LoRaWan files of the I-Cube LoRaWan V1.1.2. I tried to send Continuous waves but it doesn't work.

 

My code is :

 

int main (void){

   HAL_Init();

 

  /* USER CODE BEGIN Init */

 

  /* USER CODE END Init */

 

  /* Configure the system clock */
  SystemClock_Config();
 
  /* USER CODE BEGIN SysInit */

 

  /* USER CODE END SysInit */

 

  /* Initialize all configured peripherals */
  MX_RTC_Init();
  MX_GPIO_Init();
  MX_NVIC_Init();
  MX_SPI2_Init();
  MX_ADC_Init();
  /* Initialize interrupts */

 

  /* USER CODE BEGIN 2 */
  hardware_init();
 
  HW_Init(); 

 

   RadioEvents.TxTimeout = OnRadioTxTimeout;
  Radio.Init( &RadioEvents );

 

  test12 = Radio.Read(0x01);
  Radio.SetTxContinuousWave( 868000000, 20, 65535 );
  test12 = Radio.Read(0x01);
  Radio.Send(NULL,0);
    while (1);

}

 

But it does not work. When I read the value of the first register, I have 0x08. Any ideas to help me ?

 

Best regards,

Jérémy

Outcomes