AnsweredAssumed Answered

Additional analog inputs while using FOC library

Question asked by texgabry on Jul 17, 2013
Latest reply on Jul 18, 2013 by texgabry
Hi, I'm planing to use the FOC library (using v3.3) for a brushless motor.
The library takes care itself for the input for current (dual insulated current sensor), voltage, temperature, but it takes all the two ADC of the stm32f103 md chip.
What i the most correct way to make an application that samples also some other slow-changing analog input? Maybe a potentiometer for the speed of a fan, an input for the internal/external temperature...
Any help would be appreciated, thanks!!

Outcomes