S. Marsanne

P-L496G-CELL02

Discussion created by S. Marsanne Employee on Oct 8, 2017
Latest reply on Apr 10, 2018 by S. Marsanne

P-L496G-CELL02

STM32L496 LTE Cat M1/NB1/2G Global Cellular to Cloud Discovery Pack

Dedicated repository for related hints, tips, constructive questions and feedback.

Related image 

As LTE Cat M1/NB1 is under deployment, check regularly on the Discovery Packs C2C concierge portal for Modem SW upgrades, ensuring best functionality. Latest Modem SW Upgrade available: BG96MAR02A06M1G coming soon: BG96MAR02A07M1G

 

1. Global Quectel LTE IoT Cat M1/NB1/2G BG96 Cellular modem

2. Micro SIM socket and eSIM preprovisionned with EMnify partner complimentary data plan for largest 2G coverage while Cat M1/NB1 is being deployed (user shall source a compatible microSIM to use LTE Cat M1/NB1)

3. Open free trial account from Cloud Partners

4. Download demo binary files, drag and flash the board to test them from the STM32-C2C concierge portal

5. Discover live coding using Espruino based Javascript engine on STM32

6. Develop C-based prototype applications using STM32 Cube Expansions (X-CUBE-CLD-GEN, coming soon X-CUBE-CELLULAR, coming upgrade to X-CUBE-WATSON, X-CUBE-AZURE, X-CUBE_AWS)

7. Add differentiated feature using the available Arduino Shield, such as X-NUCLEO-IKS01A2 for sensors

8. Discovery Pack Owner's C2C Specific Portal to Activate Services and download Precompiled Demos

9. CELL01 and CELL02 are highly HW and SW compatible to reduce Time to Debug and launch:

   - Start with CELL01 to validate a project, then upgrade with CELL02 to switch to LTE IoT.

   - Use CELL01 as debugging reference plateform for quick application bug tracking on CELL02 

 

LTE Cat M1/NB1 Deployment Map

STMod+ Details and Connectors pinout

For 2G/3G version, see P-L496G-CELL01 

 

STM32 Ecosystem Partners and Contributors for STM32-C2C :

 

 

AVSystem zero-touch device to cloud pairing demo downloadable from the STM32-C2C Activation Portal

 

 Very first disco pack adopters: If the SW modem version is BG96MAR02A05M1G, make sure the modem is in factory preset user condition mode by sending the following AT command : AT+CFUN=1 to get proper connectivity. The Discovery Pack User manual shows a simple method on how to do so. The Discovery Pack is mature, FCC/RED certified.

 

BG96 Key Specification

Frequency

BG96

LTE

FDD-LTE

B1/ B2/ B3/ B4/ B5/ B8/ B12/ B13/ B18/ B19/ B20/ B26/ B28

TDD-LTE

B39 (for Cat M1 only)

EGPRS

850/900/1800/1900Mhz

Region

Global

Certification

CE/GCF/FCC/PTCRB/Verizon/AT&T/T-Mobile*/RCM/Telstra/ IFETEL/IC/BELL*/Telus*/JATE*/TELEC*/KDDI*/KC*/SKT*/CCC

Outcomes