AnsweredAssumed Answered

How to Add A Linked File Resource in System Workbench for STM32?

Question asked by martin.sergio on Oct 5, 2017
Latest reply on Oct 13, 2017 by Vangelis Fortounas

Hi,

I´m using a STM32F469I_Eval and in the Examples provides with STM32Cube_FW_F4, I can see that there are some Linked Resources (FILES). If I edit the .project file there are something like that:

 

<link>
<name>Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal.c</name>
<type>1</type>
<locationURI> copy_PARENT1/Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal.c</locationURI>
</link>

<link>
<name>Drivers/BSP/STM32469I_EVAL/stm32469i_eval.c</name>
<type>1</type>
<locationURI>copy_PARENT1/Drivers/BSP/STM32469I_EVAL/stm32469i_eval.c</locationURI>
</link>

 

But if I want to create my own project I only can create a Linked Resource (FOLDER). If I edit the .project there are something like that:

 

<link>
<name>HAL</name>
<type>2</type>
<location>C:/workspace/SystemWorkbenchForSTM32/STM32F4xx_HAL_Driver</location>
</link>

<link>
<name>STM3246I_EVAL</name>
<type>2</type>
<location>C:/workspace/SystemWorkbenchForSTM32/STM32469I_EVAL</location>
</link>

 

How can I link a File Resource like does ST? (without editing the .project file) I can´t find this option in eclipse menus

Thanks in advance,

Sergio

Outcomes