AnsweredAssumed Answered

Selft Test Library with HAL library

Question asked by Jean Paul Talledo Vilela on Oct 5, 2017
Latest reply on Oct 5, 2017 by Imen D

Hello

 

I had been using old HAL Libraries from 2015 with Selt Test Library. I just upgrade my HAL library but now I am having issues with some code changes/missing functions/definitions for the Self Test Library.  Can anyone point me out where I can get an updated STL (Self Test Library) that is compatible with the latest HAL library?

 

Some errors I am getting are related to:

 

Error[Pe135]: class "IWDG_HandleTypeDef" has no member "State" ..\STM32F4xx\Libraries\STM32_SelfTest_Library\src\stm32fxx_STLstartup.c 587


Error[Pe020]: identifier "HAL_IWDG_STATE_RESET" is undefined


Error[Pe020]: identifier "HAL_IWDG_Start" is undefined
Error[Pe135]: class "WWDG_HandleTypeDef" has no member "State"
Error[Pe020]: identifier "HAL_WWDG_STATE_RESET" is undefined
Error[Pe020]: identifier "HAL_WWDG_Start" is undefined
Error while running C/C++ Compiler
stm32fxx_STLtranspRam.c  

Outcomes