AnsweredAssumed Answered

SPWF01SA - Setting the IP Address

Question asked by cooke.ernest on Oct 4, 2017

Hi,

 

I have recently just started working on Wi-Fi code on the SPWF01SA module using the STM32F1 Nucleo Development Board.

 

I was able to get the various configuration values from the Wi-Fi module using the functions below.

 

 

And I displayed these values in HyperTerminal as can be seen below:

 

Is it possible to change the IP address of the module from the default value (192.168.0.58) to another IP address?

 

If it is possible, can someone explain to me how it is done?

 

Thank You,

Ernest

Outcomes