AnsweredAssumed Answered

Please help

Question asked by ibrahim c.p on Oct 2, 2017
Latest reply on Oct 2, 2017 by Clive One

 I have a mother board of audio, video and gps with STM8S207K6 MCU that is working condition. When I try to read eeprom from the device, the message will appear "Can not communicate with the device.

Check the swim cable connection and check all the needed pin connection or the swim connecter
If the application code uses swim desable and reset pin as out put or has desabled swim clock driver
Try now to switch off and on the application power while nrst pin forced low" 

All pins are connected with same as mentioned . 

Pins of Swim, Nrst, VDD and GND. 

Outcomes