AnsweredAssumed Answered

STM32F373 measuring VBAT with internal ADC1

Question asked by Andreas Fecht on Oct 3, 2017
Latest reply on Nov 20, 2017 by Zhitai Liu

Hello,

 

I'm using a STM32F373VCT6 and I have a problem with VBAT and ADC.

 

I have connected a CR2032 Batterie to the VBAT-Pin.
The RTC works fine with the batterie when the main power ist lost.

 

But if I try to measure the VBAT-Voltage with the internal ADC1 I get always 0.

 

The sampling on all other channels works fine; only the ADC_CHANNEL_VBAT gives this value.

 

Is there anyting else to do to measure the VBAT-voltage with the internal ADC1?

 


I'm working with CubeMX4.22.1 and CUBE V1.9.0.

 


Best regards

 

Andreas

Outcomes