AnsweredAssumed Answered

Deinitialize USB_OTG_FS

Question asked by Arsenii Soitu on Oct 2, 2017
Latest reply on Oct 5, 2017 by Arsenii Soitu

Hello!

I use cube usb library for usb_otg_fs mode wit STM32L467. I would like to use DM and DP pins also as GPIO INPUT PULL UP when usb is not used.

After usb connection closed, I do the following:

1) I use functions USBD_Stop and USBD_DeInit

2) Disable usb_otg_fs clock

2) Initialize DM and DP pins as GPIO INPUT PULL UP

But after these operations I cannot see high logic level on these pins. Maybe I didn't clear all necessary registers in usb_otg_fs? How should I properly deinitialize usb interface for using DM and DP pins as gpio?

Thank you

Outcomes