AnsweredAssumed Answered

DfuseDemo on Ubuntu using Wine

Question asked by Madhu R on Sep 29, 2017
Latest reply on Oct 9, 2017 by Madhu R

Hi ,

       I am using DfuseDemo for flashing .dfu on to my stm32l476 based board. This is working fine in the windows 7 environment. But , now to build my code i switched linux ubuntu, so i tried installing the Dfuse demo on ubuntu through wine. The installation is correct, but when i connect my board to PC, DfuseDemo is not able to detect my device.

Even , It is detected by the ubuntu as /dev/ttyUSB0, also i can see using "lsusb" command as "STMicroelectronics STM Device in DFU Mode" .

 

But  dfuseDemo, running on the wine not able to detect the device.

 

Please help me to resolve the issue.

 

Thanks and regards,

R Madhu.

Outcomes