AnsweredAssumed Answered

STM32F769I-Disco Some examples cannot start the debugger

Question asked by Anthony Verbeck on Sep 29, 2017

A few details first:

  1. Development System: Ubuntu 17.04, 64-bit
  2. Target: STM32F769I-Disco (ST-Link firmware ST-Link/V2-1 V2J29M18)
  3. IDE: Eclipse Oxygen.1 with Ac6 plug-ins
  4. STM32Cube_FW_F7_V1.8.0

I can load the projects into Eclipse by setting the workspace directory to the ws4stm32 directory in the project then importing the project. Everything builds fine. I can also download the STM32F769 by dragging the bin file to the the DIS_F769NI USB "device". Everything here works fine.

 

However, when I attempt to start the debugger (bug icon -> Debug As -> Ac6 STM32 C/C++ Application) Eclipse wedges hard. I have to kill the window to get started again. This doesn't happen with all examples. One project where it happens is the ../STM32Cube_FW_F7_V1.8.0/Projects/STM32F769I-Discovery/Examples/BSP/.

 

It seems like there's something missing or incorrectly configured.

So here are my questions:

  1. Has anyone else experienced this issue?
  2. Has anyone worked out a solution?

 

 

Thanks in advance,

ACV

Outcomes