AnsweredAssumed Answered

SPWF04S Firmware 1.1.0

Question asked by fidias lothes on Sep 28, 2017
Latest reply on May 12, 2018 by Michael Myers

Hello,
I was planning to use the SPWF04S module in a product where all the processing is done in the stm32F439 embedded in the module. It seems like the only way to load an application code is to go through the uPython interpreter. 
I need to make simple http POST/GET calls with uPython. It seems like this is only gonna be supported in 1.1.0. 
So is there any way to get this firmware, or some date when will it be available? 
Also is it possible to add the application code to the firmware on the stm32F439 ? 

Thank you!

Outcomes