AnsweredAssumed Answered

Three or one stm32f413 wakeup pin(s) from standby?

Question asked by Age Zijderveld on Sep 27, 2017
Latest reply on Sep 28, 2017 by Age Zijderveld

Dear all,

 

What are the wakeup pins of the STM32F413VGT? CubeMX and the reference manual says three (PA0/PC0/PC1) but the generated code won't accept PC0 and PC1. And when I write directly into the PWR_CSR register for the two pins, PA0 stops waking up the MCU out of standby. I'm a little bit confused, have I missed an imported part?

 

Kind regards,

 

Age

Outcomes