AnsweredAssumed Answered

stm32f769i_discovery.h(315): error:  identifier "uint32_t" is undefined

Question asked by THIHA KYAW on Sep 26, 2017

Hi,

 

When I add stm32f769i_discovery.h, I got the following error.

compiling stm32f7xx_hal_msp.c...
..\Drivers\BSP\STM32F769I-Discovery\stm32f769i_discovery.h(307): error: #20: identifier "uint32_t" is undefined
uint32_t BSP_GetVersion(void);
..\Drivers\BSP\STM32F769I-Discovery\stm32f769i_discovery.h(315): error: #20: identifier "uint32_t" is undefined
uint32_t BSP_PB_GetState(Button_TypeDef Button);

 

Please help me how I can solve it.

I use keil 5.

 

Regards,

Thiha Kyaw

Attachments

Outcomes