AnsweredAssumed Answered

frequency capture

Question asked by zine.ihab on Jun 6, 2013
im trying to capture frequency from 0 to 100khz optical encoder . and here is my code doesn't seem to work. any help please im new to micro controller.

#include "stm32f10x.h"
#include "stm32f10x_tim.h"
#include "stm32f10x_rcc.h"
#include "stm32f10x_gpio.h"
#include "misc.h"


unsigned int IC2Value,     DutyCycle ,Frequency ;




         void RCC_Configuration(void)
         {
           RCC_APB1PeriphClockCmd (RCC_APB1Periph_TIM3, ENABLE); // clock configuration
          //RCC_APB2PeriphClockCmd (RCC_APB2Periph_GPIOA, ENABLE);
         RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC | RCC_APB2Periph_AFIO, ENABLE);
         }


         void GPIO_Configuration(void)
         {
           // GPIO configuration




          GPIO_InitTypeDef   GPIO_InitStructure;
          GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7;
          GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
          GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
          GPIO_Init(GPIOC, &GPIO_InitStructure);


           GPIO_PinRemapConfig( GPIO_FullRemap_TIM3, ENABLE );        // Map TIM3 to GPIOC
         }


         void NVIC_Configuration(void)
         {
          // NVIC configuration
          NVIC_InitTypeDef       NVIC_InitStructure;
          NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn;
          NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
          NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
          NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
          NVIC_Init (& NVIC_InitStructure);
         }


         void TIM3_Configuration(void)
         {
          // TIMER configuration
          //TTIM_ICInitStructure (& TIM_ICInitStructure);
          TIM_ICInitTypeDef  TIM_ICInitStructure;
          TIM_ICInitStructure.TIM_Channel = TIM_Channel_2; // channel selection
          TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; // rising edge of the trigger
          TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; // correspondence between the pin and register
          TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; // input prescaler. Control in the number of input cycle time capture, if
          //TIM_ICInit(TIM3 , &TIM_ICInitStructure);
               /* Input signal frequency has not changed, will not change the measured period. Such as divided by 4,
                * each of the four input period before doing a capture,
                *so that the input signal does not change frequently,
               *Can reduce the frequency and software are constantly interrupted. */


               TIM_ICInitStructure.TIM_ICFilter = 0x0; // filter settings, go through several cycles transition finds the stable waveform 0x0 to 0xF


               TIM_PWMIConfig (TIM3, & TIM_ICInitStructure); // the parameter configuration TIM peripheral information


               TIM_SelectInputTrigger (TIM3, TIM_TS_TI2FP2); // select IC2 always trigger source


               TIM_SelectSlaveMode (TIM3, TIM_SlaveMode_Reset) ;// TIM mode: update event triggers the rising edge of the signal to re-initialize the counter and trigger register


               TIM_SelectMasterSlaveMode (TIM3, TIM_MasterSlaveMode_Enable); // start the timer passive trigger


               TIM_Cmd (TIM3, ENABLE); // start TIM3
               TIM_ITConfig (TIM3, TIM_IT_CC2, ENABLE); // Open interrupt
         }


int main(void)
{
       RCC_Configuration();


       GPIO_Configuration();


       TIM3_Configuration();


       NVIC_Configuration();


                    void TIM3_IRQHandler (void)
                    {




                    IC2Value = TIM_GetCapture2 (TIM3); // read IC2 capture register, the count value is the PWM cycle


                    if (IC2Value != 0)
                         {


                              DutyCycle = (TIM_GetCapture1 (TIM3) * 100) / IC2Value; // read IC1 to capture the value of the register, and calculate the duty cycle


                              Frequency = 24000000 / IC2Value; // calculate the PWM frequency.
                         }
                    else
                         {
                              DutyCycle = 0;
                              Frequency = 0;
                         }


                    TIM_ClearITPendingBit (TIM3, TIM_IT_CC2); // clear interrupt pending bit TIM




                    }
               
          while(1) {}
}

Attachments

Outcomes