AnsweredAssumed Answered

STM32 dual regular simultaneous mode with DMA

Question asked by mirk.hjl on Sep 23, 2017
Latest reply on Oct 4, 2017 by Imen D

I have a STM32F303K8T6 uC and would like to read ADC1 and ADC2 with DMA, triggered by TIM2 at the same time instance. The triggering by TIM2 works fine, but then only ADC1 is read out and not ADC2. Any suggestions what I need to change? Also when I set the adc_array to uint32_t, the upper and the lower bits are still only from ADC1.

Reference: http://www.st.com/content/ccc/resource/technical/document/reference_manual/4a/19/6e/18/9d/92/43/32/DM00043574.pdf/files/DM00043574.pdf/jcr:content/translations/en.DM00043574.pdf

main.c:

/* Includes ------------------------------------------------------------------*/#include "main.h"#include "stm32f3xx_hal.h"/* USER CODE BEGIN Includes *//* USER CODE END Includes *//* Private variables ---------------------------------------------------------*/ADC_HandleTypeDef hadc1;ADC_HandleTypeDef hadc2;DMA_HandleTypeDef hdma_adc1;DMA_HandleTypeDef hdma_adc2; SPI_HandleTypeDef hspi1;DMA_HandleTypeDef hdma_spi1_rx;DMA_HandleTypeDef hdma_spi1_tx; TIM_HandleTypeDef htim2;TIM_HandleTypeDef htim16; UART_HandleTypeDef huart1;DMA_HandleTypeDef hdma_usart1_tx;/* USER CODE BEGIN PV *//* Private variables ---------------------------------------------------------*/uint16_t adc_array[100];uint16_t adc_array2[100];char *buff_tx[64];int k=0;/* USER CODE END PV *//* Private function prototypes -----------------------------------------------*/void SystemClock_Config(void);static void MX_GPIO_Init(void);static void MX_DMA_Init(void);static void MX_TIM2_Init(void);static void MX_USART1_UART_Init(void);static void MX_SPI1_Init(void);static void MX_TIM16_Init(void);static void MX_ADC1_Init(void);static void MX_ADC2_Init(void);void HAL_TIM_MspPostInit(TIM_HandleTypeDef *htim); /* USER CODE BEGIN PFP *//* Private function prototypes -----------------------------------------------*//* USER CODE END PFP *//* USER CODE BEGIN 0 *//* USER CODE END 0 */int main(void){   /* USER CODE BEGIN 1 */   /* USER CODE END 1 */   /* MCU Configuration----------------------------------------------------------*/   /* Reset of all peripherals, Initializes the Flash interface and the Systick. */  HAL_Init();   /* USER CODE BEGIN Init */   /* USER CODE END Init */   /* Configure the system clock */  SystemClock_Config();   /* USER CODE BEGIN SysInit */   /* USER CODE END SysInit */   /* Initialize all configured peripherals */  MX_GPIO_Init();  MX_DMA_Init();  MX_TIM2_Init();  MX_USART1_UART_Init();  MX_SPI1_Init();  MX_TIM16_Init();  MX_ADC1_Init();  MX_ADC2_Init();   /* USER CODE BEGIN 2 */    //TIMER    HAL_TIM_OC_Start_IT(&htim2,TIM_CHANNEL_1) ; //Start Timer 2, Channel 1    HAL_TIM_OC_Start_IT(&htim2,TIM_CHANNEL_2) ; //Start Timer 2, Channel 2    HAL_TIM_OC_Start_IT(&htim2,TIM_CHANNEL_3) ; //Start Timer 2, Channel 3    HAL_TIM_OC_Start_IT(&htim2,TIM_CHANNEL_4) ; //Start Timer 2, Channel 4      //ADC DMA    HAL_ADCEx_Calibration_Start(&hadc1,ADC_SINGLE_ENDED);    HAL_ADCEx_Calibration_Start(&hadc2,ADC_SINGLE_ENDED);     //HAL_ADC_Start_DMA(&hadc1, (uint16_t*)adc_array, 100);    HAL_ADCEx_MultiModeStart_DMA(&hadc1, (uint16_t*)adc_array, sizeof(adc_array));   /* USER CODE END 2 */   /* Infinite loop */  /* USER CODE BEGIN WHILE */  while (1)  {      k++;      if(k>10000) {          sprintf(buff_tx,"voltage=%d,Ia=%d\n",adc_array[0],(adc_array[1]));          usart_tx(&huart1,64,buff_tx);          k=0;      }  /* USER CODE END WHILE */   /* USER CODE BEGIN 3 */   }  /* USER CODE END 3 */}/** System Clock Configuration */void SystemClock_Config(void){   RCC_OscInitTypeDef RCC_OscInitStruct;  RCC_ClkInitTypeDef RCC_ClkInitStruct;  RCC_PeriphCLKInitTypeDef PeriphClkInit;     /**Initializes the CPU, AHB and APB busses clocks      */  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;  RCC_OscInitStruct.HSIState = RCC_HSI_ON;  RCC_OscInitStruct.HSICalibrationValue = 16;  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;  RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL4;  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }     /**Initializes the CPU, AHB and APB busses clocks      */  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK                               |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;   if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }   PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_ADC12;  PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK1;  PeriphClkInit.Adc12ClockSelection = RCC_ADC12PLLCLK_DIV1;  if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }     /**Configure the Systick interrupt time      */  HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);     /**Configure the Systick      */  HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);   /* SysTick_IRQn interrupt configuration */  HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);}/* ADC1 init function */static void MX_ADC1_Init(void){   ADC_MultiModeTypeDef multimode;  ADC_ChannelConfTypeDef sConfig;     /**Common config      */  hadc1.Instance = ADC1;  hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;  hadc1.Init.Resolution = ADC_RESOLUTION_12B;  hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;  hadc1.Init.ContinuousConvMode = DISABLE;  hadc1.Init.DiscontinuousConvMode = DISABLE;  hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;  hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T2_TRGO;  hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;  hadc1.Init.NbrOfConversion = 1;  hadc1.Init.DMAContinuousRequests = ENABLE;  hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;  hadc1.Init.LowPowerAutoWait = DISABLE;  hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;  if (HAL_ADC_Init(&hadc1) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }     /**Configure the ADC multi-mode      */  multimode.Mode = ADC_DUALMODE_REGSIMULT;  multimode.DMAAccessMode = ADC_DMAACCESSMODE_12_10_BITS;  multimode.TwoSamplingDelay = ADC_TWOSAMPLINGDELAY_2CYCLES;  if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }     /**Configure Regular Channel      */  sConfig.Channel = ADC_CHANNEL_4;  sConfig.Rank = 1;  sConfig.SingleDiff = ADC_SINGLE_ENDED;  sConfig.SamplingTime = ADC_SAMPLETIME_601CYCLES_5;  sConfig.OffsetNumber = ADC_OFFSET_NONE;  sConfig.Offset = 0;  if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }}/* ADC2 init function */static void MX_ADC2_Init(void){   ADC_ChannelConfTypeDef sConfig;     /**Common config      */  hadc2.Instance = ADC2;  hadc2.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;  hadc2.Init.Resolution = ADC_RESOLUTION_12B;  hadc2.Init.ScanConvMode = ADC_SCAN_DISABLE;  hadc2.Init.ContinuousConvMode = DISABLE;  hadc2.Init.DiscontinuousConvMode = DISABLE;  hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;  hadc2.Init.NbrOfConversion = 1;  hadc2.Init.DMAContinuousRequests = ENABLE;  hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV;  hadc2.Init.LowPowerAutoWait = DISABLE;  hadc2.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;  if (HAL_ADC_Init(&hadc2) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }     /**Configure Regular Channel      */  sConfig.Channel = ADC_CHANNEL_1;  sConfig.Rank = 1;  sConfig.SingleDiff = ADC_SINGLE_ENDED;  sConfig.SamplingTime = ADC_SAMPLETIME_181CYCLES_5;  sConfig.OffsetNumber = ADC_OFFSET_NONE;  sConfig.Offset = 0;  if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }}/* SPI1 init function */static void MX_SPI1_Init(void){   /* SPI1 parameter configuration*/  hspi1.Instance = SPI1;  hspi1.Init.Mode = SPI_MODE_MASTER;  hspi1.Init.Direction = SPI_DIRECTION_2LINES;  hspi1.Init.DataSize = SPI_DATASIZE_8BIT;  hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;  hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;  hspi1.Init.NSS = SPI_NSS_SOFT;  hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;  hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;  hspi1.Init.TIMode = SPI_TIMODE_DISABLE;  hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;  hspi1.Init.CRCPolynomial = 7;  hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;  hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;  if (HAL_SPI_Init(&hspi1) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }}/* TIM2 init function */static void MX_TIM2_Init(void){   TIM_ClockConfigTypeDef sClockSourceConfig;  TIM_MasterConfigTypeDef sMasterConfig;  TIM_OC_InitTypeDef sConfigOC;   htim2.Instance = TIM2;  htim2.Init.Prescaler = 0;  htim2.Init.CounterMode = TIM_COUNTERMODE_CENTERALIGNED3;  htim2.Init.Period = 200;  htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;  htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;  if (HAL_TIM_Base_Init(&htim2) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }   sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;  if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }   if (HAL_TIM_PWM_Init(&htim2) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }   sMasterConfig.MasterOutputTrigger = TIM_TRGO_OC4REF;  sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;  if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }   sConfigOC.OCMode = TIM_OCMODE_PWM1;  sConfigOC.Pulse = 0;  sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;  sConfigOC.OCFastMode = TIM_OCFAST_ENABLE;  if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }   if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }   if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }   sConfigOC.Pulse = 100;  if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_4) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }   HAL_TIM_MspPostInit(&htim2);}/* TIM16 init function */static void MX_TIM16_Init(void){   TIM_OC_InitTypeDef sConfigOC;  TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig;   htim16.Instance = TIM16;  htim16.Init.Prescaler = 20;  htim16.Init.CounterMode = TIM_COUNTERMODE_UP;  htim16.Init.Period = 7400;  htim16.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;  htim16.Init.RepetitionCounter = 0;  htim16.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;  if (HAL_TIM_Base_Init(&htim16) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }   if (HAL_TIM_OC_Init(&htim16) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }   sConfigOC.OCMode = TIM_OCMODE_TIMING;  sConfigOC.Pulse = 0;  sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;  sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;  sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;  sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;  sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;  if (HAL_TIM_OC_ConfigChannel(&htim16, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }   sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;  sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;  sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;  sBreakDeadTimeConfig.DeadTime = 0;  sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;  sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;  sBreakDeadTimeConfig.BreakFilter = 0;  sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;  if (HAL_TIMEx_ConfigBreakDeadTime(&htim16, &sBreakDeadTimeConfig) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }}/* USART1 init function */static void MX_USART1_UART_Init(void){   huart1.Instance = USART1;  huart1.Init.BaudRate = 57600;  huart1.Init.WordLength = UART_WORDLENGTH_8B;  huart1.Init.StopBits = UART_STOPBITS_1;  huart1.Init.Parity = UART_PARITY_NONE;  huart1.Init.Mode = UART_MODE_TX_RX;  huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;  huart1.Init.OverSampling = UART_OVERSAMPLING_16;  huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;  huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;  if (HAL_UART_Init(&huart1) != HAL_OK)  {    _Error_Handler(__FILE__, __LINE__);  }}/**    * Enable DMA controller clock   */static void MX_DMA_Init(void) {  /* DMA controller clock enable */  __HAL_RCC_DMA1_CLK_ENABLE();   /* DMA interrupt init */  /* DMA1_Channel1_IRQn interrupt configuration */  HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);  HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);  /* DMA1_Channel2_IRQn interrupt configuration */  HAL_NVIC_SetPriority(DMA1_Channel2_IRQn, 0, 0);  HAL_NVIC_EnableIRQ(DMA1_Channel2_IRQn);  /* DMA1_Channel3_IRQn interrupt configuration */  HAL_NVIC_SetPriority(DMA1_Channel3_IRQn, 0, 0);  HAL_NVIC_EnableIRQ(DMA1_Channel3_IRQn);  /* DMA1_Channel4_IRQn interrupt configuration */  HAL_NVIC_SetPriority(DMA1_Channel4_IRQn, 0, 0);  HAL_NVIC_EnableIRQ(DMA1_Channel4_IRQn);  /* DMA1_Channel6_IRQn interrupt configuration */  HAL_NVIC_SetPriority(DMA1_Channel6_IRQn, 0, 0);  HAL_NVIC_EnableIRQ(DMA1_Channel6_IRQn);}/** Configure pins as          * Analog          * Input          * Output         * EVENT_OUT         * EXTI */static void MX_GPIO_Init(void){   GPIO_InitTypeDef GPIO_InitStruct;   /* GPIO Ports Clock Enable */  __HAL_RCC_GPIOA_CLK_ENABLE();  __HAL_RCC_GPIOB_CLK_ENABLE();   /*Configure GPIO pin Output Level */  HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET);   /*Configure GPIO pin Output Level */  HAL_GPIO_WritePin(GPIOA, GPIO_PIN_15, GPIO_PIN_SET);   /*Configure GPIO pin : PA6 */  GPIO_InitStruct.Pin = GPIO_PIN_6;  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;  GPIO_InitStruct.Pull = GPIO_NOPULL;  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);   /*Configure GPIO pin : PA15 */  GPIO_InitStruct.Pin = GPIO_PIN_15;  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;  GPIO_InitStruct.Pull = GPIO_PULLUP;  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);}/* USER CODE BEGIN 4 *//* USER CODE END 4 *//**   * @brief  This function is executed in case of error occurrence.   * @param  None   * @retval None   */void _Error_Handler(char * file, int line){  /* USER CODE BEGIN Error_Handler_Debug */  /* User can add his own implementation to report the HAL error return state */  while(1)    {  }  /* USER CODE END Error_Handler_Debug */ }#ifdef USE_FULL_ASSERT /**    * @brief Reports the name of the source file and the source line number    * where the assert_param error has occurred.    * @param file: pointer to the source file name    * @param line: assert_param error line source number    * @retval None    */void assert_failed(uint8_t* file, uint32_t line){  /* USER CODE BEGIN 6 */  /* User can add his own implementation to report the file name and line number,     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */  /* USER CODE END 6 */}#endif/**   * @}   */  /**   * @} */  /************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

HAL_ADC_MspInit() in stm32f3xx_hal_msp.c:

 

void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc){   GPIO_InitTypeDef GPIO_InitStruct;  if(hadc->Instance==ADC1)  {  /* USER CODE BEGIN ADC1_MspInit 0 */   /* USER CODE END ADC1_MspInit 0 */    /* Peripheral clock enable */    HAL_RCC_ADC12_CLK_ENABLED++;    if(HAL_RCC_ADC12_CLK_ENABLED==1){      __HAL_RCC_ADC12_CLK_ENABLE();    }     /**ADC1 GPIO Configuration         PA3     ------> ADC1_IN4      */    GPIO_InitStruct.Pin = GPIO_PIN_3;    GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;    GPIO_InitStruct.Pull = GPIO_NOPULL;    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);     /* ADC1 DMA Init */    /* ADC1 Init */    hdma_adc1.Instance = DMA1_Channel1;    hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY;    hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE;    hdma_adc1.Init.MemInc = DMA_MINC_ENABLE;    hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;    hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;    hdma_adc1.Init.Mode = DMA_CIRCULAR;    hdma_adc1.Init.Priority = DMA_PRIORITY_MEDIUM;    if (HAL_DMA_Init(&hdma_adc1) != HAL_OK)    {      _Error_Handler(__FILE__, __LINE__);    }     __HAL_LINKDMA(hadc,DMA_Handle,hdma_adc1);   /* USER CODE BEGIN ADC1_MspInit 1 */   /* USER CODE END ADC1_MspInit 1 */  }  else if(hadc->Instance==ADC2)  {  /* USER CODE BEGIN ADC2_MspInit 0 */   /* USER CODE END ADC2_MspInit 0 */    /* Peripheral clock enable */    HAL_RCC_ADC12_CLK_ENABLED++;    if(HAL_RCC_ADC12_CLK_ENABLED==1){      __HAL_RCC_ADC12_CLK_ENABLE();    }     /**ADC2 GPIO Configuration         PA4     ------> ADC2_IN1     PA5     ------> ADC2_IN2      */    GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5;    GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;    GPIO_InitStruct.Pull = GPIO_NOPULL;    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);     /* ADC2 DMA Init */    /* ADC2 Init */    hdma_adc2.Instance = DMA1_Channel2;    hdma_adc2.Init.Direction = DMA_PERIPH_TO_MEMORY;    hdma_adc2.Init.PeriphInc = DMA_PINC_DISABLE;    hdma_adc2.Init.MemInc = DMA_MINC_ENABLE;    hdma_adc2.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;    hdma_adc2.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;    hdma_adc2.Init.Mode = DMA_CIRCULAR;    hdma_adc2.Init.Priority = DMA_PRIORITY_MEDIUM;    if (HAL_DMA_Init(&hdma_adc2) != HAL_OK)    {      _Error_Handler(__FILE__, __LINE__);    }     __HAL_LINKDMA(hadc,DMA_Handle,hdma_adc2);   /* USER CODE BEGIN ADC2_MspInit 1 */   /* USER CODE END ADC2_MspInit 1 */  }}

Outcomes