AnsweredAssumed Answered

Maximum output current value of PWM, TIM

Question asked by Ken Inoue on Sep 16, 2017
Latest reply on Sep 18, 2017 by Ken Inoue

Sorry for my poor English.

What is the maximum output current value of PWM using TIM? Where can I find it in the data sheet? I am using STM32F334. I am investigating whether the MOSFET can be directly driven by the PWM from the microcomputer without the gate driver.

On page 78/121 of the data sheet of STM32F334x4 STM32F334x6 STM32F334x8, the following description was given

 

Is IIO=8mA, 20mA the PWM maximum output current value? Which is 8 mA or 20 mA?

 

Best Regards,

Ken Inoue

Outcomes