AnsweredAssumed Answered

STM32CubeL4 1.9.0 CubeMx 4.22.1

Question asked by alex on Sep 14, 2017
Latest reply on Sep 16, 2017 by alex

There might be an ADC clock issue when the project is configured with CubeMx 4.22.1 and 1.9.0 CubeL4.
When SAI clock is selected for ADC in CubeMx the HAL_RCCEx_PeriphCLKConfig called by SystemClock_Config returns HAL_ERROR.
Everything works if SYSCLK is selected as ADC clock##.
SAI clock configuration works correctly with the previous versions of CubeMx and CubeL4 libraries.

Outcomes