AnsweredAssumed Answered

Is possible to turn off power of the ST-Link board on my Nucleo F411RE without cut it off?

Question asked by donnarumma.gian_paol on Sep 15, 2017
Latest reply on Sep 15, 2017 by Uwe Bonnes

I'm working with a Nucleo F411RE.

I've setted JP5 to E5V than I have power up the board from VIN pin. 

My Chip and application works well, but the STLINK board still working without USB. I can see the Red Led (LD1) flashing.

If I measure power consumption on IDD connector I read 13mA, but If I read power consumption direcly from E5V I read 70mA.

 

Is possible to turn off the STLINK without cut it off from the board?

 

Really thank you.

Outcomes