AnsweredAssumed Answered

Issues with lwIP and debugging

Question asked by user 143 on Sep 14, 2017
Latest reply on Sep 19, 2017 by user 143

Hello,

I need your help. I've got some troubles with lwIP and to find a solution for that I want to enable debugging in lwIP. 

I'm working with a STM3210C-EVAL board and with CubeMX. lwIP is working, I can send a ping and also see the webpage in fsdata. But now I want to enable debugging. I also configured UART2 with CubeMX and can send messages via HAL_UART_Transmit(). Then I redirect printf, so that messages are send via UART. This also workes fine. For this I added this lines to my main.c:

 

#ifdef __GNUC__
/* With GCC, small printf (option LD Linker->Libraries->Small printf
set to 'Yes') calls __io_putchar() */
#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
#else
#define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f)
#endif /* __GNUC__ */

 

And after the main function:

PUTCHAR_PROTOTYPE {
HAL_UART_Transmit(&huart2, (uint8_t *)&ch, 1, 0xFFFF);
return ch;
}

 

And now I wanted to enable the debugging in lwIP. For this, I added the lines below in lwipopts.h:

#define LWIP_DEBUG 1

#define ICMP_DEBUG LWIP_DBG_ON

 

But there are no messages send when I ping or open the webserver. I tried another options, like IP_DEBUG or TCP_DEBUG, but there is no difference. 

 

Have anyone an idea where my mistake is?

 

Thank you

Outcomes