AnsweredAssumed Answered

STM32F0x devices and HTTPS client

Question asked by Francisco SinapseEnergia on Sep 14, 2017
Latest reply on Sep 14, 2017 by Clive One

STM32 MCUs Forum 

 

(I don't know if i write the post in right sub-forum place).

 

I face to one issue to get data from one server using port 443. HTTPS for getting data instead HTTP. (First at all , I am newbie with secure connection protocol).

 

I am using one typical wifi gateway (i.e:HLK-RM08S). This is connected to one TX/RX STM32F030CC UART and then we send data to server..

 

Now, for getting valid data from server, we use one script developed under python. ( h2 = httplib2.Http(timeout=30, disable_ssl_certificate_validation=True). I understand that this means that data is sent without encrypting. is it?. We want do same process with one STM32F030CC instead this python script.

 

How I can face to this issue?. Does exist one library that I can import and it is valid for STM32F030CC device (in general STM32F0xx family?.

 

Thanks in advance!

 

Best regards.

Outcomes