AnsweredAssumed Answered

[CubeMX regression]Failed to generate code with 4.22.1

Question asked by marton.miklos on Sep 13, 2017
Latest reply on Sep 15, 2017 by marton.miklos

The new CubeMX 4.22.1 fails to generate code (and hangs on generation) for a STM32 workbench project which has been successfully generated with the previous versions.

 

Here is the command line output from the problem:

[Bash] mm@mm-imac:~$ /opt/STM32CubeMX/STM32CubeMX log4j user configuration file not f - Pastebin.com 

 

I am using Linux please see the ioc file attached. The error also occurs when generating blank project.

Attachments

Outcomes