AnsweredAssumed Answered

STM32F071RB stdperiph_lib support ?

Question asked by Sebastian J. on Sep 11, 2017
Latest reply on Sep 11, 2017 by Clive One

Hey,

does someone use stdperiph_lib V1.5 in combination with stm32f071rb ?

 

Just read in the changelog that it was updated in Dec. 2015:

  • Add support of the STM32F070xB, STM32F070x6 and STM32F030xC  devices.

But did not find anything regarding to stm32f071rb.

 

Is there a solution or is the cpu only fully supported inside the HAL of CubeMx ?

 

Regards

 

Sebastian

Outcomes