AnsweredAssumed Answered

STM32L152C- Discovery "target halted due to breakpoint" while running

Question asked by Development DGOC on Sep 11, 2017
Latest reply on Sep 12, 2017 by Development DGOC

Hi, I am using the STM32L152C- Discovery.

I am trying to run an example project from STM32CubeL1, however , I get the following error while running.

 

** Programming Started **
auto erase enabled
Info : Device: STM32L1xx (Cat.1 - Low/Medium Density)
Info : STM32L flash size is 128kb, base address is 0x8000000
STM32L152RCTx.cpu: target state: halted
target halted due to breakpoint, current mode: Thread
xPSR: 0x61000000 pc: 0x2000000e msp: 0x20008000
wrote 8192 bytes from file Debug/STM32L152C-Discovery.elf in 0.614524s (13.018 KiB/s)
** Programming Finished **
** Verify Started **
STM32L152RCTx.cpu: target state: halted
target halted due to breakpoint, current mode: Thread
xPSR: 0x61000000 pc: 0x2000002e msp: 0x20008000
verified 4152 bytes in 0.061745s (65.668 KiB/s)
** Verified OK **
** Resetting Target **
adapter speed: 240 kHz
shutdown command invoked

Outcomes